AXIS#.SAFEPARAM.SSM_#.VELLOWERLIMIT

Description

Indicates the velocity lower limit of the Safe Speed Monitor (SSM) safety function.

 

This is n_LL_SSM in the following diagram:

Context

For complete SSM information refer to SSM (Safe Speed Monitor).

Related safety parameters:

Versions

Action

Version

Notes

Implemented

2-04-00-000

Implemented in SMM revision v0.56

General Information

Type

Read/Write

Units

Depends on user units

Range

[-2^31+1, 2^31-1]
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
AXIS1.SAFEPARAM.SSM_1.VELLOWERLIMIT

315fh

02h

Signed32

-

-

Read/Write

No

AXIS1.SAFEPARAM.SSM_2.VELLOWERLIMIT

3160h

02h

Signed32

-

-

Read/Write

No

AXIS2.SAFEPARAM.SSM_1.VELLOWERLIMIT

325fh

02h

Signed32

-

-

Read/Write

No

AXIS2.SAFEPARAM.SSM_2.VELLOWERLIMIT

3260h

02h

Signed32

-

-

Read/Write

No